Skip to main content
Visitor II
September 18, 2008
Question

ERASE FLASH

  • September 18, 2008
  • 3 replies
  • 983 views
Posted on September 18, 2008 at 02:24

ERASE FLASH

    This topic has been closed for replies.

    3 replies

    newsamoAuthor
    Visitor II
    May 29, 2008
    Posted on May 29, 2008 at 10:28

    I'm working on st10f168 with st10flasher, now, load monitor is ok, dump is ok, but i'm not able to program flash because appears error messagea boute flash erase: EraseFlash failed.flash

    How can i erase ?

    Visitor II
    June 2, 2008
    Posted on June 02, 2008 at 07:05

    Hello Newsamo,

    Programming voltage (12V) of the on-chip Flash memory must be supplied to pin VPP(pin 84).

    Is the 12V ensured in this pin during programming/erasing operation?

    Best regards,

    Najoua.

    Visitor II
    September 18, 2008
    Posted on September 18, 2008 at 02:24

    Hello Najoua,

    in which others microcontrollers of st10fxxx family I need to apply the voltage programming to erase and program?

    Thank you !!!