Skip to main content
Visitor II
June 13, 2007
Question

error with a scattered file

  • June 13, 2007
  • 2 replies
  • 742 views
Posted on June 13, 2007 at 15:33

error with a scattered file

    This topic has been closed for replies.

    2 replies

    Visitor II
    June 13, 2007
    Posted on June 13, 2007 at 08:04

    Hi there,

    I want to use a scattered file for my project but I have the following error messages:

    Undefined symbol Image$$RO$$Limit (referred from 71x_init.o)

    Undefined symbol Image$$RW$$Base (referred from 71x_init.o)

    Undefined symbol Image$$ZI$$Base (referred from 71x_init.o)

    Undefined symbol Image$$ZI$$Limit (referred from 71x_init.o)

    Do I have to modify the startup file init.s to reimplement __user_intial_stackheap() or it’s another problem ? I am a little confused :D

    Can someone please advise. Thanks in advance.

    simple.scf

    FLASH 0x40000000 0x40000

    {

    BOOT 0x40000000 0x40000

    {

    71x_vect.o (Vect, +First)

    71x_init.o (Init)

    * (+RO)

    }

    RAM 0x20000000 0xC000

    {

    * (+RW)

    * (+ZI)

    }

    }

    Visitor II
    June 13, 2007
    Posted on June 13, 2007 at 13:30

    everything works fine, I have to put these symbols in comment in the startup file. sorry.

    best regards,

    hkaesse