EVSPIN32F0601S1 not running motor
Hi All,
I am trying to get up and running the above hardware. I downloaded the software for the board, and we already use IAR compiler here. After compiling and downloading (via the STLink), the system runs the program just fine.
However, I just need to run the system with the onboard POT and it is not moving or energizing the motor at all.
I changed the 6step_conf.h file to POTENTIOMETER_INTERFACE = 1 and all others to 0. Nothing happens.
All the voltages to the board are perfect (running 70VDC to the board via a 7 amp programmable power supply).
All help would be greatly appreciated. This is my first intro into using the part. Time is very tight.
regards,
Charles