sometimes when I'm exiting the power down mode via P2.5, the ST10F276 does not use the external clock but it's basic frequeny (~1MHz), although there's no problem with the RPD delay(~13ms) or the crystal. I do see the external clock when passing the 2.5V at RPD. I'm using a 8MHz crystal and the P0H7..5 are set to ''110'' I guess the PLL determines wheather there is a stable external clock or not after the RPD delay, correct? [ This message was edited by: RK on 06-04-2006 11:29 ]