Skip to main content
Visitor II
October 24, 2003
Question

External 8 bits Mux RAM

  • October 24, 2003
  • 2 replies
  • 625 views
Posted on October 24, 2003 at 08:07

External 8 bits Mux RAM

    This topic has been closed for replies.

    2 replies

    jmAuthor
    Visitor II
    October 22, 2003
    Posted on October 22, 2003 at 06:44

    Hi,

    I work on st10f168, and i want to connect external RAM to it using EBC

    But in 8 bits MUX mode, i don't know which port is use to datas and adress.

    So if you use it in the same configuration, give me a answer

    THANKS a lot

    bye

    Visitor II
    October 24, 2003
    Posted on October 24, 2003 at 08:07

    The data are on port P0L and the addresses on P0, P1 and eventually P4. for more detail have a look at the ST10x167 user's manual.

    (ST10R167 and ST10F168 are fully compatible except for the program memory)

    http://www.stmcu.com/mcdfiles/7317.pdf