You need to use PSD outputs, PB, PC etc Configure a pin each for A12, A13, A14, A15 as chipselect, active high. Then in the next part, Chip Select Equations, enter the signal for the chip select in the Logical AND box example: A12 , no start address, no end address, a12 in the Logical AND box hope this helps Simon [ This message was edited by: sjh on 12-11-2003 16:20 ]
Address lines a12 - a15 used for the xRAM can be brought out externally by using ports pb0 - pb3 of the uPSD. Just set these pin to ''Combinatorial'' CPLD output, then write an I/O Logic equation for each of the a12-a15 pins, (e.g. a12_x=a12, a12 output enable=Vcc). After the *.obj is loaded to your uPSD, pb0 will become your address line, a