Hello, I want to use the external interrupts INT2, INT3, INT4 and INT5 of the STR710 uC.(as inetrrupt only no wake-up)
But for some reason I can not configure the XTI_ registers. I added the following to my STR710.h file: /* ****************************************** */ /* External interrupt definitions */ /* ****************************************** */ #define XTI_BASE 0xE0001000 #define XTI_SR (*(REG32 IOPORT2_BASE+7)) #define XTI_CTRL (*(REG32 IOPORT2_BASE+9)) #define XTI_MRH (*(REG32 IOPORT2_BASE+10)) #define XTI_MRL (*(REG32 IOPORT2_BASE+11)) #define XTI_TRH (*(REG32 IOPORT2_BASE+12)) #define XTI_TRL (*(REG32 IOPORT2_BASE+13)) #define XTI_PRH (*(REG32 IOPORT2_BASE+14)) #define XTI_PRL (*(REG32 IOPORT2_BASE+15)) In the initialisation of my main.c I wrote the following: XTI_MRH = 0; // wake-ups 7-15 disabled XTI_MRL = 0; // wake-ups 0-6 disabled XTI_PRL = 0; // clear all interrupt flags XTI_TRH = 0; // wake-up on falling edge XTI_TRL = 0; // wake-up on falling edge XTI_CTRL &= 0xFFFE; // wake-up disabled XTI_CTRL |= 0x0002; //External interrupts enabled XTI_SR = 0; // no software interrupts (I also enabled channel 5 of the EIC.) However, external interrupts of my eval board are not working. If I look in the memory during XTI initilisation nothing happens. Is this why the external interrupts don't work. My ISR() look like: void XTI_IRQ_isr ( void ) { SWITCH_IRQ_TO_SYS; /* BEGIN USER CODE XTI_IRQ */ IOPORT2_PD ^= 0x8000; //toggle led XTI_PRH = 0; // resets perhiperal interrupts XTI_PRL = 0; // resets external interrupts 2 till 5 /* END USER CODE XTI_IRQ */ SWITCH_SYS_TO_IRQ; // clear IRQ Pending bit EIC_IPR0 = CHANNEL(5); } Has somebody any suggestions? Regards, Jimmey