I have a big doubt with the LVD specifications for the ST72F262:
In a former datasheet (Dec. 2003) I found that LVD works with Vdd max. rise time of 100ms/V; now the new release of the datasheet states that max. rise time is 20ms/V. We have 900 boards already assembled, and Vdd rise time is 40ms/V: is it still a safe value for the LVD to work properly ? Can anybody explain what could happen internally if the rise time is too slow ? We have only a 100nF capacitor between Reset and GND, no pullup resistor. Thank you
Yes, it was an error in the datasheet(100ms/V). Actually it was 100ms/5Volt => 20ms/V. I think with 40ms/V, the functioning may not be guaranted but should be ok if you do not use pull up on reset.