Skip to main content
Visitor II
January 26, 2006
Question

field firmware update & serial Port

  • January 26, 2006
  • 22 replies
  • 3107 views
Posted on January 26, 2006 at 09:21

field firmware update & serial Port

    This topic has been closed for replies.

    22 replies

    Visitor II
    January 9, 2006
    Posted on January 09, 2006 at 05:57

    I found appnote AN2078 STR71x In-Application Programming using UART.

    ''The maximum size of the image to be loaded: 56 Kbytes.''

    meaning STR712FR2 (code 256 KB) can be program up to 56Kbyte?,buy STR712FR1 (code 128 KB) is better ?

    [ This message was edited by: kmaster on 09-01-2006 10:31 ]

    Visitor II
    January 9, 2006
    Posted on January 09, 2006 at 06:13

    Hello,

    In fact this application note will be updated in next few weeks. The new version of the AN2078 will allows the user to program all the 256KB.

    I think to by an STR712FR2 or an STR712FR1 does not depends on the AN2078 but depends on the user application resources. Because the AN2078 is an application note, not a bootloader, and the user has to load the application note code using a specified flasher tool then run it.

    Thanks.

    [ This message was edited by: Bouha on 09-01-2006 10:46 ]

    Visitor II
    January 9, 2006
    Posted on January 09, 2006 at 06:44

    First production will use STR712FR2 and install IAP/bootloader via JTAG.

    In field (After sale service) will programming via PC-RS232.

    Waiting for new IAP(AN2078)...

    [ This message was edited by: kmaster on 09-01-2006 11:17 ]

    Visitor II
    January 9, 2006
    Posted on January 09, 2006 at 10:18

    Is AN2078 also available for the IAR compiler?

    THX

    Bertl

    Visitor II
    January 9, 2006
    Posted on January 09, 2006 at 12:03

    Actually the AN2078 is available for RVDK toolset.

    Thanks

    Visitor II
    January 16, 2006
    Posted on January 16, 2006 at 23:52

    How long to launch new version (New-IAP program all flash) ??

    Can be use JTAG-wiggler to program STR712FR2 ??

    Visitor II
    January 17, 2006
    Posted on January 17, 2006 at 04:45

    A new version is planned to be published on STMCU website in week 7.

    Find attached a beta version of this application note which is under validation.

    Please Let me know if there is something wrong 8-)

    ________________

    Attachments :

    IAP_V2.0.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtEE&d=%2Fa%2F0X0000000aKX%2F9qoG2lRxbBMi_.JsMqlVg_6QdSRkAnwhbBAf_qmM9xw&asPdf=false
    Visitor II
    January 17, 2006
    Posted on January 17, 2006 at 08:10

    ST have a future product (STR7xx) that support On-Chip bootloader (like P89C51RD2 ) ??

    User can program via JTAG or UART0 available for low price programmer.

    Commercial JTAG $100-$1000, RS232(UART0) $5.

    Visitor II
    January 18, 2006
    Posted on January 18, 2006 at 04:08

    For more information about the STR7xx products, contact your nearest distributor or ST sales office.

    Visitor II
    January 18, 2006
    Posted on January 18, 2006 at 17:54

    Hi,

    Are you sure the code posted has not the 56k limitation?

    I saw few differences in source code with previous version.

    I am trying to make it work with CrossStudio, but I am having trouble with my app remaping. Do you have any source example?

    Regards,

    Leo