Skip to main content
Visitor II
March 12, 2004
Question

File .wed and .wdb

  • March 12, 2004
  • 3 replies
  • 1061 views
Posted on March 12, 2004 at 08:57

File .wed and .wdb

    This topic has been closed for replies.

    3 replies

    dspadoni9Author
    Visitor II
    March 10, 2004
    Posted on March 10, 2004 at 12:42

    We're using ST7MDT20-DVP3 development sistem and the visual debug generates project.wed and project.wdb files. These files become more and more large and slow down the debug remarkablly. It is possible to eliminate these files every time that the project is compiled?

    Thanks.

    Visitor II
    March 11, 2004
    Posted on March 11, 2004 at 01:11

    Hi danspando,

    Below is the model mak file in which you can add commands to remove the wed and wdb files. Hope this will help u.

    PATHC = C:\Metrowerks\CodeWarrior_STM_V1.1

    APPLI = example

    LK_CMD_FILE = $(APPLI).prm

    # List of source files

    C_SRC_LIST = start07.c timer.c

    ASM_SRC_LIST =

    CC = ''$(PATHC)\prog\cst7.exe''

    AS = ''$(PATHC)\prog\ast7.exe''

    LK = ''$(PATHC)\prog\linker.exe''

    INCDIR = ''$(PATHC)\lib\st7c\include''

    CFLAGS = -Lasm -ml -i$(INCDIR)

    AFLAGS =

    LFLAGS = -envGENPATH=$(PATHC)\lib\st7c\lib

    CP = copy

    RM = del

    # List of object files from list of source files

    OBJ_LIST = $(patsubst %.c,%.o,$(filter %.c,$(C_SRC_LIST)))

    $(patsubst %.asm,%.o,$(filter %.asm,$(ASM_SRC_LIST)))

    # Rules for building targets

    $(APPLI).abs: $(OBJ_LIST) $(LK_CMD_FILE)

    $(LK) $(LFLAGS) $(LK_CMD_FILE)

    # Other rules for compiling C and asm files

    %.o : %.c

    $(CC) $(CFLAGS) $<

    %.o : %.s

    $(AS) $(AFLAGS) $<

    # Rule for forcing the build without taking into account dependencies

    rebuild:

    gmake -f $(APPLI).mak clean

    gmake -f $(APPLI).mak $(APPLI).abs

    clean :

    if exist $(APPLI).abs $(RM) $(APPLI).abs

    if exist *.o $(RM) *.o

    if exist *.ls $(RM) *.ls

    if exist *.map $(RM) *.map

    if exist *.wed $(RM) *.wed

    if exist *.wdb $(RM) *.wdb
    Visitor II
    March 12, 2004
    Posted on March 12, 2004 at 08:57

    You must know that if you delete these you will lose environment information and the workspace will open in edit and debug modes with certain ''default'' windows open.