Skip to main content
Visitor II
April 1, 2004
Question

Flash memory

  • April 1, 2004
  • 2 replies
  • 477 views
Posted on April 01, 2004 at 21:43

Flash memory

    This topic has been closed for replies.

    2 replies

    ricardofAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:59

    with the emulation board with the uPSD3334, when I download the flash, where is recorded this flash, in the primary flash or in the second or where ?

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:59

    If you are using PSDsoft to program your flash, it depends on your settings. Go to the ''Merging of MCU or DSP firmware with PSD'' settings. There you will find each ''Memory Select Name'' and an optional ''File Name'' associated with it. If the ''File Name'' field contains a hex file name, then the flash memory associated with the ''Memory Select Name'' will be programmed.