Skip to main content
Visitor II
July 6, 2005
Question

Floating analog inputs

  • July 6, 2005
  • 3 replies
  • 836 views
Posted on July 06, 2005 at 17:16

Floating analog inputs

    This topic has been closed for replies.

    3 replies

    web55604Author
    Visitor II
    July 5, 2005
    Posted on July 05, 2005 at 12:13

    Hi

    I am using an ST72F324 with analog inputs on port D

    When in power down mode, the input to these ports can be an arbritary value.

    This causes the digital input buffer to consume power - up to 200 microamps.

    Is there any way to switch this off ?

    Are the input buffers isolated only when ADC conversion takes place ?

    Visitor II
    July 6, 2005
    Posted on July 06, 2005 at 02:22

    As recommended in the datasheet, there shall not be any floating inputs. It is adviced to put a pull-up or pull-dn on these pins.

    What do you mean by power-dn mode ? BTW, PortD pins do not have external interrupt capability. Yu can try reducing power consumption by enabling the internal pull-up.

    web55604Author
    Visitor II
    July 6, 2005
    Posted on July 06, 2005 at 17:16

    Port D is multiplexed with the ADC analog inputs.

    They may be driven by an arbritary analog value.

    If this is done, the P and N transistors of the inputs buffer may both saturate leading to a higher power consumption.

    The device is powered down in full HALT mode.

    I am also using an external low voltage detact device (device LVT disabled) and real time clock/alarm, so the total system drain is around 6 uA. The target is