Skip to main content
Visitor II
June 22, 2004
Question

Generate 2KHz by timer interrupt

  • June 22, 2004
  • 2 replies
  • 634 views
Posted on June 22, 2004 at 05:11

Generate 2KHz by timer interrupt

    This topic has been closed for replies.

    2 replies

    alanlai1Author
    Visitor II
    June 14, 2004
    Posted on June 14, 2004 at 14:09

    Dear Sir ~

    I am using ST6242, using interrupt to generate the toggle frequency.

    (Target = 2kHz square wave for buzzer).

    But I can not get the excected frequency.

    My setting:

    TSCR = 01101XXXB (XXX = PS0:2)

    PSC = 0XXXXXXXB (XXXXXXX=)

    TCR = 00000001B

    My expect and determination:

    Shortest Interrupt interval should be = 1 / (4Mhz / 12 / 1 ) = 3us

    / 12 means divide by 12 (refer to ST6242 spec page 18/70)

    /128 means divide by 128 (refer to ST6242 spec page 41/70)

    Shortest square freq = 1 / [3us (Hi) + 3us (Lo)] = 166kHz

    PS(0:2)=000,PSC(0:7)=00000000>Result Freq=166kHz,interval=3us

    My result:

    PS(0:2)=000,PSC(0:7)=00000000>Result Freq=500Hz, interval=843us

    PS(0:2)=001,PSC(0:7)=00000000>Result Freq=309Hz, interval=1.6ms

    PS(0:2)=010,PSC(0:7)=00000000>Result Freq=158Hz, interval=3ms

    PS(0:2)=011,PSC(0:7)=00000000>Result Freq=80Hz, interval=6ms

    PS(0:2)=100,PSC(0:7)=00000000>Result Freq=40Hz, interval=12ms

    PS(0:2)=101,PSC(0:7)=00000000>Result Freq=800Hz, interval=562us

    PS(0:2)=110,PSC(0:7)=00000000>Result Freq=1.2kHz, interval=386us

    PS(0:2)=111,PSC(0:7)=00000000>Result Freq=1.0kHz, interval=456us

    In my testing above, I cannot find a setting can meet my expectation.

    Is it my concept wrong? Can you please help in coding?

    My Tools=ST6240B-EMU2, Compiler=RIDE

    Thanks

    Best Regards

    Lai
    Visitor II
    June 22, 2004
    Posted on June 22, 2004 at 05:11

    With the TCR you can the 500Hz multiply by 4! so you can make 2Khz.

    But for the calculation for the timers, i use always an excel sheet. It's an automatic calculation after delay time insertion.

    I attached the excel sheet.

    ________________

    Attachments :

    ST6-Timer.xls : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Ev&d=%2Fa%2F0X0000000bXK%2FN_qhflHQ5TTpim4nY6SBletov2oJMvgIeq08B_Q4KP8&asPdf=false