Skip to main content
Visitor II
October 9, 2008
Question

GPIO speed

  • October 9, 2008
  • 3 replies
  • 988 views
Posted on October 09, 2008 at 05:54

GPIO speed

    This topic has been closed for replies.

    3 replies

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:51

    Now I run PLL at 96MHZ PLL and FLASH at 48MHZ, when I set one GPIO from

    0->1->0, it takes about 400ns... is it normal?

    But if I calculate the ideal speed of it, it should be less than 50ns, right? Because I need to use GPIO to simulate parallel port data/address... now the actual speed of GPIO is too slow... Is anyone know how to improve it? Please kindly give me advices.

    Thank you very much.

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:51

    Hi

    See:

    '' TARGET=''_blank''>

    http://www.st.com/mcu/forums-cat-4852-html

    >

    6MHz square wave (12MHz toggle)is achievable.

    Regards

    Mark

    http://www.uTasker.com

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:51

    Hello,

    I develop an application with the STR9-Comstick. The idea is to control the I/O ports with a program in Visual Basic through the USB-B connector near the pins of I/O ports.

    Which dll use for that for the enumeration ?

    The first application will be to generate a TTL signal for differents frequencies through a pin of the I/O ports. Is there a way to program it in C (TTL signal) for the STR9 ? And so the program in VB ?

    Regards

    Vlieghe Guillaume