Skip to main content
Visitor II
February 21, 2008
Question

H-JTAG Issue

  • February 21, 2008
  • 4 replies
  • 1172 views
Posted on February 21, 2008 at 03:07

H-JTAG Issue

    This topic has been closed for replies.

    4 replies

    rajugnvAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:49

    Hi,

    I am trying to connect STR912 based target(self made PCB) board with Parallel Port Based Jtag hardware.

    This is first time I am working on STR9. I am unable to detect target device through H-JTAG.

    I am facing following problems..

    I have kept TAP configuration as suggested in H-JTAG User Manual Fig 3-12

    TAP Num – 0 IReg Len – 5

    TAP Num – 1 IReg Len – Auto

    TAP Num – 2 IReg Len – 8

    Iam getting device id as 0x12CB3020

    When the TAP configuration is not done I got 0x02471E40

    Both are invalid device ids.

    In site link

    http://www.hjtag.com/pic/TAPConfig.jpg

    a different TAP configuration is mentioned like this.

    TAP Num – 1 IReg Len – 5

    TAP Num – 1 IReg Len – Auto

    TAP Num – 1 IReg Len – 8

    I have not yet tried out this TAP configuration.

    Please let me know which is correct.

    Is Target Reset is must as shown in Fig:3-11.

    And also can I use nSRST instead of nTRST to reset target hardware for the figure shown in 3-11 of H-JTAG user manual as I do not have support for nTRST in my JTAG hardware.

    By seeing the change of Device ID received when TAP configuration is changed can I ensure chip is working to some extent.

    Please let me know how I could proceed further in these circumstances.

    Thanks in advance for the support,

    rajugnvAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:49

    The device has been detected using the configuration

    TAP Num – 1 IReg Len – 5

    TAP Num – 1 IReg Len – Auto

    TAP Num – 1 IReg Len – 8

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:49

    hi, rajugnv

    have you succeeded to program either of the flash of STR91x with h-jtag? how to? thank you!

    best regards

    tsyejay

    rajugnvAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:49

    NO. I could not. We are Using Keil ULINK to do it.