I'm trying to work with the HD44780-based LCD-module. When I'm using an emulator (Visual Micro Lab), it seems to be ok - there is such object in the program, so I can see the status of the LCD-module, it's initialized, and I can display any messages. But if I burn this program to work with the real LCD-module (ST6220F, ST6220C), I donn't have any results - the module seems to be not working (I've tried 3 modules, so the problem is not the defect display). If anybody has worked this LCD-modules, it will be very kind to send me an initialize procedure.
I've used them a lot. Can you give some info: 1. the connections you are using? 2. what type of display 16x2, 20x4 etc? 3. are you using 4bit or 8bit mode? I'll post some code - it will be for the raisonance tool Simon [ This message was edited by: sjh on 12-11-2003 16:22 ]
That's the answers: 1. pb3-pb0 - data lines (D8-D5) pb7 - RS pb5 - RW pb6 - E 2. 16*2 3. 4 bit If it's possible, could you send the example connection of V+, GND and contrast, I'm not sure in the connection I did With best regards, Aleksej