Skip to main content
Visitor II
July 29, 2003
Question

HELP ! Cable power off

  • July 29, 2003
  • 8 replies
  • 1334 views
Posted on July 29, 2003 at 14:01

HELP ! Cable power off

    This topic has been closed for replies.

    8 replies

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:55

    I'm trying to send my program to the evaluation board DK3200 via Jtag Port but it' doesn't work.

    when I test the JTAG : loop test : OK

    connect test : failed

    I had once this message : device is secured but I never protected the µPSD.

    somebody can help me, please.

    Totof.
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:55

    When the Connect Test failed, it should generate a log file, connect.log, and a txt file, connect.txt, in the PSDsoft Express temp directory. Can you please send these files to me for analysis? Also which version of PSDsoft Express are you using? Are the JTAG pins PC0, PC1, PC5 and PC6 dedicated for JTAG use only, or are you using them in multiplex mode? Also have you tried to send an ''erase'' cmd and see if it works?

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:55

    hi,

    I link in attachement the connect.txt and connect.log files. My PSDSoft Express version is Version 7.91.

    The 6 Jtag pins PC0, PC1,... are only dedicated to the Jtag Port.

    The erase and anything else do the same thing and the same error :

    JTAG-ISP Operations : The Part is incorrect (Instruction Register)

    Thanks for your help!

    totof.

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:55

    The Connect.txt you sent says the ''Power is off''. When the power is applied to your board, do you see the clock input to the uPSD oscillating? If your hardware checks out O.K. and you still can not talk to your DK3200 board, you can zip up your PSDsoft project folder and send it to

    mailto:apps.psd@st.com

    so that I can take a look at it.
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:55

    Thanks for your reply.

    I have tried you said and I have a 36 MHz clock on XTAL 1, and i have the same error message ''Cable power off''

    totof

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:55

    Hello,

    Indeed, Vcc = 3V !!!

    The LT1962 (U5) is burned !! Vin(pin

    =12V Vout(pin1) = 3V !!

    I have changed the LT1962 regulator so VCC_1 is 5V now and the JTAG Port works, the code is transmitted !! but the uPSD don't works correctly !! I'm disapointed because I can't follow my work, I can't drive the mcu port correctly and so on.

    Totof

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:55

    Check Vcc input to uPSD and make sure it is within the operating range. If Vcc is O.K., check if the /Reset to uPSD is functional.

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:55

    It looks like the defective voltage regulator also took the uPSD on your board. We will send you a new DK3200 board. Please send back the old one after you received the new board.