Posted on May 17, 2011 at 09:53Hello, to create a new project,open the Hitop. 1)in the ''using projects in Hitop'', click on create ''a new project from a template''. 2)choose your compiler and your micricontroller. 3) The project will be made with a default settings (compiler,assembler and linker), you can use this configuration. 4) add your source file and don't forget to add the path of the header files(Project->settings->tools settings->include directories). 5) to generate an elf file set the extension of the target name to .elf(from project->settings->tools settings->general->target name) - Attached you find a preconfigured project with tasking compliler (It should be better to download the latest version of hitop-arm (5.30)) regards, mgd.
HI all.Does anybody know/using HiTOP IDE then please help me.
Tell me the procedure to create new application.I face some problem with creating elf file,symbol preprocessor.I fail to generate .elf, .htx and .sym . Ide ask for elf at start only. So, if anybody knows tell me the complete procedure to create new project , then new application, IDE configuration, compilation and linking. Best regards Sai
But didnt got any help from it.There is no option ''using projects in Hitop'' as such. Iam using HiTOP52-ARM Version-05.20.0310 So please give me further detail. Best regarg sai [ This message was edited by: sr_shinde on 24-06-2008 12:06 ]
the ''using projects in Hitop'' is a window which appears when opening Hitop. you can find all the necessary information in the Hitop online help(in the section ''getting started->starting up the system->starting hitop'' mgd,