Hi, Was planning to implement a design based on STUSB4500. have some queries about the working of STUSB4500 under different conditions.
1. If we are using A_B_Side for Super speed MUX selection, whether this A_B_side will be available on following
a) if a USB2.0 or Type A connected to Type C port using a USB2.0 or Type A to Type C connector.
b)Whether ATTACH or A_B_Side is suitable for Highspeed MUX selection for pin selection for High speed communication.
2.if OTG device is connected to Type C port, will the STUSB block the VBUS to be applied to the peripheral through Type C. (Connecting External Hard disk using OTG in the Type C port)