High optimization of IAR Embedded Workbench 9.60.3
What does the 'High' optimization actually do in IAR Embedded Workbench 9.60.3 when the 'Size' option is selected, but no additional optimization checkboxes are enabled. Even without selecting any extra options(like CSE, loop unrolling, etc. ), the code size reduces significantly—up to 30%. How is the IAR Embedded Workbench 9.60.3 achieving this reduction, and what specific optimizations are being performed in this case.