Skip to main content
Visitor II
June 19, 2018
Question

High side switch VN7003ALH in parallel

  • June 19, 2018
  • 1 reply
  • 945 views
Posted on June 19, 2018 at 16:51

Hello,

I'm interested in developing an application involving the high side switch VN7003ALH. In particular I was interested in putting more of these switches in parallel in order to split the current load. In order to read the total current that flows through the switches will it be sufficient to use a voltage summer with an op-amp that receives the CS pin output currents?

Is there other attentions to be aware in a parallel configuration?

Thank you very much,

Best regards,

Matteo

#vn7003 #high-side-switch #current #parallel #power
    This topic has been closed for replies.

    1 reply

    Visitor II
    June 25, 2018
    Posted on June 25, 2018 at 16:25

    Hello Matteo,

    paralleling VN7003ALH devices is not recommended only in case of inductive loads. For all other cases, further information can be found in the 'VIPower® M0-7 standard high-side drivers hardware design guide', Chapter 8, at the following link:

    https://www.st.com/content/ccc/resource/technical/document/user_manual/group0/13/bb/11/4c/95/7c/4a/d0/DM00214136/files/DM00214136.pdf/jcr:content/translations/en.DM00214136.pdf

     

    Best regards,

    Luigi

    Visitor II
    June 25, 2018
    Posted on June 25, 2018 at 17:13

    Hello Luigi,

    Thanks for the reply. In my application I have a single battery, so a single VBat and single GND reference point. Therefore put CS pins in parallel should be ok.

    In my case VN7003ALH is not driving directly an inductive load, but will instead act as a cut off switch for the power supply of electronics which drive the inductive load so that the demagnetization energy will discharge through their power path.

    Best regards,

    Matteo