I'd like to know how I can address the ''Long'' RAM (ST7 Lite19 from 0100 to 017F, on Memory Map-->16-bit Addressing RAM). I tryed with : LD X,$01 LD A,($FF,X) but the ST Visual Develop send me a message with (no existent memory at address 0x0100). Is the same with : LD X,$00 LD A,($0100,X) Many tanks MKBS
3 REGISTER & MEMORY MAP There you'l finde the text : The available memory locations consist of 128
bytes of register locations, 256 bytes of RAM, 128
bytes of data EEPROM and 4 Kbytes of flash program
memory. The RAM space includes up to 128
bytes for the stack from 180h to 1FFh.
.....
IMPORTANT: Memory locations marked as “Reserved�
must never be accessed. Accessing a reseved
area can have unpredictable effects on the
device.You can't use the reserved area from 100 to 1FF. But if you need more RAM it is possible to address the unused (!) part of the so called 'stack' area e.g. from 180 to 19F. Regards WoRo
Make sure you have a 16bit ram section defined, eg.
WORDS ; don't alocate all 16bit ram, save some for the stack segment byte at 180-1A0 'ram' ; define some data bytes segment 'ram' .test DS.B 1 then use the data clr A ld test, A Regards sjo[ This message was edited by: sjo on 20-09-2004 10:57 ]