How can I apply small loads to the output of TDA7377?
According to the TDA7377 datasheet, the standby pin 7 must have currents smaller than 5 mA. I am using the dual bridge configuration and have applied a 10 ohm load across pins 1 and 2 and the amplifier works great. If I want to output 2 A of current (pins 1 and 2) and a resistance of about 1 ohm, how can I drive a small load like that?
From the datasheet, it seems that the standby pin would not allow such a small load. From page 6 of the datasheet, it says that the standby pin avoids the device being turned on when a resistive path of less than 16 ohms is present between the output and ground, but I need to support a load of 1 ohm between pins 1 and 2.
The chip is on a pre-purchased PCB. Can I just disconnect pin 7 from the rest of the pins to be able to drive this small load?
Thank you.