How do I configure and load the STNRGPF01?
Helo,
I have recently bought a STEVAL-IPFC01P1, to evaluate de STNRGPF01 controller.
Besides some issues with the power stage, I still wonder how can I configure the hex code into the chip.
In the datasheet it is mentioned that it is needed a STNRG Loader along with the eDesign suite.
Is there a manual or webpage with detailed steps to configure this device? I mean, what hardware conection is necesary, where to download the Loader, and whether there is an eDesign suite downloadable to work offline with the STNRGPF01.
If I wanted to design a new power converter I see no way to configure and load the divice yet. I have looked for information in the ST web, but there is no clear enough information.
#stnrgpf01-configuration