I'm a beginner. I want to use the head file in ''C:\Program Files\STMicroelectronics\st7toolset\include\ST72F324J6.h''. But I don't know how do go to use,especial following code: /* System Integrity Control/Status Register */ STVD7_EXTERN volatile unsigned char SICSR @0x2b; define SICSR_WDGRF 0 /* Watchdog Reset Flag */ define SICSR_WDGRF_OR (1 << SICSR_WDGRF) define SICSR_LVDRF 4 /* LVD Reset Flag */ define SICSR_LVDRF_OR (1 << SICSR_LVDRF) define SICSR_AVDF 5 /* Voltage Detector Flag */ define SICSR_AVDF_OR (1 << SICSR_AVDF) define SICSR_AVDIE 6 /* Voltage Detector Interrupt */ define SICSR_AVDIE_OR (1 << SICSR_AVDIE) define SICSR_AVDS 7 /* Voltage Detection Selection */ define SICSR_AVDS_OR (1 << SICSR_AVDS) could anybody help me,please?
Here is an example using the ADC of the ST7Lite09. I hope it is clear enough.
Best regards. /* ---------------------- (c) 2003 STMicroelectronics ------------------- */ /*********************************************************/ /* This program uses the ST7FLITE09. It configures the ADC to convert on */ /* channel AIN1 (PB1), scales the value read on 4 bits and sends the result */ /* on PA0/1/2/3. */ /* With the simulator, use the ADC_Stimuli.in file as input stimuli and plot */ /* the AdcValue variable, PA0/1/2/3 and PB1 pins, run the simulator and */ /* visualize the results with the plotter. */ /****************************************************/ /* Include file provided by STVD7 describing the registers mapping. */ #define __DEFINE_REGISTERS_STVD7_INCLUDE__ #include #undef __DEFINE_REGISTERS_STVD7_INCLUDE__ /* Define Macros for bit manipulation. */ #define SetBit(VAR,BIT_NUM) ( (VAR) |= (1<#define ClrBit(VAR,BIT_NUM) ( (VAR) &= ((1<#define ValBit(VAR,BIT_NUM) ( (VAR) & (1<#define BitIsClear(VAR,BIT_NUM) ( 0 == ValBit(VAR,BIT_NUM) ) #define BitIsSet(VAR,BIT_NUM) ( !BitIsClear(VAR,BIT_NUM) ) /* Global variable */ unsigned char AdcValue; /*******************************************************/ void main(void) { /* Configures port A0/1/2/3/4 as output. */ PADDR = 0x1F; PAOR = 0x1F; PADR = 0x00; /* Enables the ADC on AIN1. */ ADCCSR = ( ADCCSR_ADON_OR | ADCCSR_CH0_OR ); while(1) { /* Waits for the end of the conversion. */ while(BitIsClear(ADCCSR, ADCCSR_EOC)); /* Reads the A/D value. */ AdcValue = ADCDR; /* Divide it in order to have it on 5 bits */ /* and writes it on the PortA. */ PADR = AdcValue >> 3; /*******************************/ } }