Skip to main content
Visitor II
August 28, 2019
Question

How ESP32 WROOM 32 interface with STM32F413 ?

  • August 28, 2019
  • 6 replies
  • 7056 views

Hello ST Team,

I'm doing interface between STM32F413 & ESP32 WROOM 32, but not getting how many pins of ESP32 WROOM 32 are going to use for interface with STM32F413.

I'll going to do UART communication.

How many program pins , data pins & control pins of ESP32 WRROM 32 are required while using ESP32 WRROM 32 as a WiFi or BLE module ??

What other settings to do while writing firmware for the same ?

Let me know as early as possible.

Thank you.

    This topic has been closed for replies.

    6 replies

    Visitor II
    August 28, 2019

    Hi,

    You can use uart driver from esp-idf SDK to handle uart at ESP32 side.

    Find more here...

    https://docs.espressif.com/projects/esp-idf/en/latest/api-reference/peripherals/uart.html

    One Application example also provided into esp idf (read above link carefully).

    SGhugAuthor
    Visitor II
    August 28, 2019

    Hello,

    Thanks to immediate response.

    I'll go through the link you provided.

    For PCB hardware side, Is MTDO, MTMS, MTDI, MTCK pins of esp32 wroom 32 connect to STM32F413 for programming to ESP32?

    Visitor II
    August 28, 2019

    Use RXD0, TXD0, IO0(BOOT to GND) and RESET(IO21) to programm the ESP Wroom module

    SGhugAuthor
    Visitor II
    August 28, 2019

    OK, get it.

    When I'm using WiFi & BLE both at same time so, Is it possible to use with single UART of ESP32 ?

    Is any hardware changes to resolve this problem or need to make changes in software?

    Visitor II
    April 9, 2021

    GPIO 16-RX1 and GPIO 17-TX1 pwr-3.3v GND are used for AT-commands

    Visitor II
    April 9, 2021

    i got how to interface ESP32 interfaced with stm32g4 using uart for ATcommands... bassically i wanted to send AT-commands to my ESp32 wroom from stm32g431RB but i could not read the return value after spending nearly 3 days i found out 3 things

    1)....the esp32 which i was using was not working properly

    2).....my stm32 was not powering my esp32 properly so i used usb cable to power my esp32 wroom...

    3).....when recieving the OK response from the ESP32 i was geeting what i sent so i increased the no. of bytes to be received more that 10 which gave me OK along with other values also...

    i used UART1 of esp32 wroom as it is for At-commands gpio16-rx1 gpio17-tx1 use usb to power the ESP32

    and comman ground ....also use usb-uart converter to see the response.. the basic example code is below .....baud rate 115200,parity-none,databits 8,stop bit-1 flow control set to 0. on both side ESP32 and STM32(the word side is 8).

    main()

    {

    init.....

    .

    .

    HAL_UART_Transmit(&huart4,(uint8_t*)"AT+RST\r\n",8,100); // for veiwing usb-uart

    HAL_UART_Transmit(&huart1,(uint8_t*)"AT+RST\r\n",8,100); // ESP32

     while (1)

     {

    HAL_UART_Receive_IT(&huart1,(uint8_t*)ret,13); // waiting for resonse

    if(HAL_UART_Receive_IT(&huart1,(uint8_t*)ret,13)==HAL_OK) //after the response is complete

    {

    HAL_UART_Transmit(&huart4,(uint8_t*)ret,13,100); // for veiwing usb-uart

    }

     }