How to configure Undervoltage Alarm (UVA) of CLT01-38SQ7
Hi, I use CLT01-38SQ7. In datasheet (DocID028182 Rev 1) is not clear to me how to use Vcs pin (24V sensor power supply sensing input) for UVA purpose.
In Figure 7. “Logic status of the SCLT3-8BQ7 power supply�? voltage ranges of Vcc and Vc are shown, but I do not understand how these values are determined, since they depend on the values of the voltage divider in the circuit Vcs (pin 14) and his input current.
NOTE: This question and answer originated from a customer support case which was handled by us. We regularly review support cases and add any helpful ones here for all to benefit from.