Skip to main content
Visitor II
September 17, 2020
Question

How to generate firmware for STNRGPF02

  • September 17, 2020
  • 0 replies
  • 694 views

Hi everyone, I'm designing an application with an STNRGPF02 and would like to generate an appropriate firmware for it.

I made the conception using the STNRGPF12 design, since the chips are very similar and the PF02 is not available through eDesignSuite (even though the documentation says otherwise), but there is (obviously) no option for the relay inrush parameters and I can't be sure that it will work properly (which I would rather know before testing a non isolated, line powered application :grinning_face_with_sweat: )

Could someone tell me the appropriate way to proceed ?

Best regards,

Julien FAUCHER

    This topic has been closed for replies.