How to make the CubeIDE generate a workspace that can be copied and renamed without issues
CubeIDE 1.7
Windows 10
We have used TrueStudio 9.3 for years without issue but because we began using a new ST STM32G070 processor, we needed to change to ST's version of CubeIDE. We have it building the project(with low level drivers included) but if we copy the workspace and then rename it, the PROJECT_LOC(under Properties-->Resource-->Linked Resources) is pointing back to the original named directory. Both PARENT_LOC and WORKSPACE_LOC are showing up linked to the new location.
I have tried numerous workspace and project settings but nothing seems to work. I've even compared the settings to the ones used in TrueStudio but they both look nearly identical.
Any help would be appreciated. Thanks