How to read the data from M95256 EEPROM?
I'm using M95256 IC which is used as an external EEPROM for the controller. When i'm sending Read Status Register command i can see data from IC in receive buffer. But when i'm sending Read from Memory command, i get only 0xFF data in the buffer.I have checked the Status register after Write to memory command and the WIP = 0 and WEL=1 in the register. I'm not able to see the data on the oscilloscope as well even though i can see Read from memory command is getting transmitted in Tx Buffer as well as i can see it on oscilloscope.