How to use the buck switching regulator ST1S03PUR, and dimension the components value for an out 3v3 and 500mA?
Hi, latelly I am trying to use the buck switching regulator ST1S03PUR and I have some problems with it. It should be something easy to do but seems like not.
I have a DC Vin 12V and i want as out 3V3 and 500mA.
For the Vout I am using the formula from datasheet VO = VFB [1 + R1 / R2].
Vfb=0,8V.
I'm a litle confused because I am following the datasheet and it is easy to put out 3v3 but once I put a load ST1S03PUR can not hold it and breaks puting in S.C Vin and GND.
Vin 12V from an lnk3206 ac/dc switching 300mA out.
For sure I'am doing something wrong and one of them is the layout of the pcb but for sure even the layout isn't the best I could do , I should not have this kind of problem.
No temperature problems detected.
Could you help me to understand what's wrong in my case?
Thank you
Leonard