Question
HVLED815PF on Power Supply eDesignSuite
Posted on November 16, 2016 at 11:30
Hi There,
It would be great to be able to choose HVLED815PF on eDesignSuite, when selecting:Power Conversion -> Power Supply -> AC/DC -> Isolated -> QR Flyback (with HPF), instead of only as LED Driver. The purpose is to use it in designs with less than 11W (actual Pout in general/home lighting produtcs) with CV, PSR, Wide Mains and HPF, instead of using the HVLED0001/A models that despite working, were made for much higher power supplies (75W). The HVLED815PF shows this kind of use (CV) on the application note:''AN4350: High power factor LED driver with constant voltage regulation based on HVLED815PF''
(that has some errors on formulas still to solve - we already submitted a request for the correction or an errata) but unfortunately the eDesignSuite doesn't seem to let us use it on the same way.
Best Regards,
Pedro Pereira
#supply #mc34063 #psr-cv #psr-cv #power #hvled815pf #hvled815pf