Skip to main content
Visitor II
May 11, 2004
Question

I failure read EPROM from st62T65B6

  • May 11, 2004
  • 2 replies
  • 844 views
Posted on May 11, 2004 at 13:54

I failure read EPROM from st62T65B6

    This topic has been closed for replies.

    2 replies

    1adcAuthor
    Visitor II
    May 11, 2004
    Posted on May 11, 2004 at 10:18

    Hello!

    My ST62T65B6 is controled PLL FM exciter.

    What for winee.exe send message ''device is protect'' when try read?

    I not another programd ST62T65 and much read program from EPROM

    How read EPROM and program ?

    Thank!

    Visitor II
    May 11, 2004
    Posted on May 11, 2004 at 13:54

    In case the Programmer works properly and the device is neither defective nor disconnected check the protection bit.

    Find the following text in the specification:

    1.3.2.1 Program Memory Protection

    The Program Memory in OTP or EPROM devices

    can be protected against external readout of memory

    by selecting the READOUT PROTECTION option

    in the option byte.

    In the EPROM parts, READOUT PROTECTION

    option can be disactivated only by U.V. erasure

    that also results into the whole EPROM context

    erasure.

    Note: Once the Readout Protection is activated, it

    is no longer possible, even for SGS-THOMSON,

    to gain access to the OTP contents. Returned

    parts with a protection set can therefore not be accepted.

    PROTECT. This bit allows the protection of the

    software contents against piracy. When the bit

    PROTECT is set high, readout of the OTP contents

    is prevented by hardware. No programming

    equipment is able to gain access to the user program.

    When this bit is low, the user program can

    be read.