Skip to main content
Visitor II
February 21, 2012
Question

I have a question about the input voltage of ALTAIR04 IN eDesign

  • February 21, 2012
  • 2 replies
  • 995 views
Posted on February 21, 2012 at 11:01

I want to design with ALTAIR04 in the software, but the input voltage must be less than 350V, I want to know that 

 it means ALTAIR04 can’t be designed in a input of 440V AC?, or it’s only the limit of the software ?

    This topic has been closed for replies.

    2 replies

    ST Employee
    February 21, 2012
    Posted on February 21, 2012 at 11:48

    Hi Peter,

    first of all thanks for your interest in eDesignStudio.

    Up to now, ALTAIR04-900 design on eDesignStudio supports input voltage lower than 350V, but we are working so that it can sustain ultra wide-range operations. You'll find this updating in next release.

    Meanwhile, you can check application note AN3290 (http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/APPLICATION_NOTE/CD00286662.pdf), where, at page 29, it's described how to modify standard schematic, as that provided by eDS, so that it can sustain even greater input voltages.

    Best regards,

    eDesignStudio team member

    Visitor II
    February 22, 2012
    Posted on February 22, 2012 at 03:20

    Hi Patrizia

    thanks for your quick response.

    I have seen the application note, expect the updated software

    Best Regards