Question
I think there is a bug in the STM32CubeIDE Version: 1.4.0 Build: 7511_20200720_0928 (UTC), section “device configuration tool ?, section STMicroelectronics.X-CUBE-TOUCHGFX.4.15.0 Mode and configuration.
When Graphics Application is checked, a folders tree starting from TouchGFX, with files like GFX2.touchgfx, etc, is generated. It’s OK.
When the .ioc file becomes complicated (as the example I attach), it seems that TouchGFX is replaced by Src and all files are generated under Src, mixing them with main.c and the other files.
Could you fix this, please?