I would like to kwow if my SM6T18A/CA on the input connector of my product is compliant with the no destruction of my electronic which is located just after when fast Transient 61000-4-4 is applied.
Hi Sir,
I currently use a SM6T18A/CA on the 12V+/- 5% power supply input of my product.
After this protection are located many electronic components with absolute maximum rating voltage levels (continuous) given from 13,2V to 18V.
After applying the transient voltage Test 61000-4-4 (+/-1KV levels), I can observe that one component is destroyed. I can not that it corresponds to the only component which is not HBM compliant (+-2KV).
All others components are compliant with HBM and are not destroyed even if I think the resulted clamping voltage on the SM6T18/CA regarding 61000-4-4 (+/-1KV levels) is over their absolute maximum rating voltage levels (continuous) given from 13,2V to 18V.
- What is the clamping voltage level on the SM6T18A/CA regarding 61000-4-4 (+/-1KV levels)?
- Is this transient clamping voltage can be considered as an issue for the electronic components after which have a maximum rating voltage levels (continuous) from 13,2V to 18V?
- May I consider that HBM (+/-2KV) is a guarantee to support the clamping voltage after the SM6T18A/CA protective diode (because all the current has been drived by the protective diode, and no much energy is still present on the 12V power supply rail)?
Thank you very much for your support.
Anthony.