I am having a hard time getting the I2C routines contained in the RTC demo firmware (dk32dsn3.zip) working properly on the dk3 I am not famiar with the I2C module (I have only used bit-banging).... and the uPSD323x datasheet Rev1.2 does not contain any information on how to USE the I2C peripheral. It only contains 4 pages on the associated registers and their descriptions.
I am confused by the use of dummy writes to the S2DAT register especially. How does S2DAT = 0xFF put the I2C peripheral into receive mode? If anyone has programming guide / flow chart for the I2C peripheral it would be a BIG help. Thanks
We will be releasing an I2C driver within a few weeks for master and slave modes that should be helpful. We will also include a demo to show how to use the drivers.
Well, that makes two of us. The I2C documentation is indeed very fuzzy and I also had a very hard time to make it work, after many trials and innumerous errors. Until ST releases something more complete, I attached my I2C module for master mode operation, without interrupt.
I hope that this will help you. By the way, I have a quite large experience with I2C: 8052 bitbang, Philips master mode and Microchip slave mode. So, I must be a complete idiot, or something is really missing in the doc. Bye, Daniel
We are working to release a uPSD3200 I2C driver that will be made available on our website (target release is within a month). A notification will be made on the forum when it is available.
On a case-by-case basis, a beta version of the I2C driver will be made available. If interested in receiving a copy of the beta version, please send a request to
mailto:apps.psd@st.com
with the following information: Name Company Name Phone Number Location (City, State, Country) uPSD part number of device being used (3234, 3254, etc.) Application Projected annual volume (units) Regards, uPSD Applications Engineering