Skip to main content
Visitor II
April 13, 2004
Question

I2C with uPSD3212

  • April 13, 2004
  • 2 replies
  • 693 views
Posted on April 13, 2004 at 10:43

I2C with uPSD3212

    This topic has been closed for replies.

    2 replies

    igorlAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:59

    Dear all!

    Can anybody help me? I tried to used I2C and came across with one problem: I set SII, then I set STA bit (start condition), then I load S2DAT register and it sends this 8-byte serie. But after it, both SDA and SCL are in ''0'' state, while they need to be at ''high-impedance'' state.

    No device is connected to I2C from another side (uPSD3212 is the only device) and interrupts are disabled. Can we try I2C in such condition? Do you have any ASM-code exampple of I2C usage?

    Thank you in advance.
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:59

    We are working to release a uPSD3200 I2C driver that will be made available on our website (target release is within a month). A notification will be made on the forum when it is available.

    On a case-by-case basis, a beta version of the I2C driver will be made available. If interested in receiving a copy of the beta version, please send a request to

    mailto:apps.psd@st.com

    with the following information:

    Name

    Company Name

    Phone Number

    Location (City, State, Country)

    uPSD part number of device being used (3234, 3254, etc.)

    Application

    Projected annual volume (units)

    Regards,

    uPSD Applications Engineering