Skip to main content
Visitor II
December 12, 2005
Question

IAP Driver Compile Error

  • December 12, 2005
  • 3 replies
  • 932 views
Posted on December 12, 2005 at 09:42

IAP Driver Compile Error

    This topic has been closed for replies.

    3 replies

    Visitor II
    December 8, 2005
    Posted on December 08, 2005 at 14:26

    Hi,

    I downloaded IAP application note from link

    http://www.st.com/stonline/products/support/micro/files/an2zip

    and opened project with realview debugger v1.7. IAP project is created with previous version of realview ide. So Realview debugger v1.7 upgrade the project. And then I build the project but

    Error: L6224E: Could not place common.o(.data) in any Execution region. error occured. What is the reason for this error? Attached zip file contains all source files and build log file.

    ________________

    Attachments :

    IAP_Driver_upgraded.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtHD&d=%2Fa%2F0X0000000aL0%2FgVzwP4O2eizyQzgI_GMahhxtWiuUgDrzU0fn9KktNeQ&asPdf=false
    Visitor II
    December 9, 2005
    Posted on December 09, 2005 at 12:49

    I did not modify any file.

    Scatter file is as follow

    FLASH 0x40000000 0x10000

    {

    FLASH 0x40000000

    {

    71x_vect.o (Vect, +First)

    71x_init.o (Init)

    * (+RO)

    }

    RAM 0x20000000

    {

    program.o (+RO)

    common.o (+RO)

    flash.o (+RO)

    uart.o (+RO)

    * (+ZI)

    }

    }

    Visitor II
    December 12, 2005
    Posted on December 12, 2005 at 09:42

    this line solve the problem but There is lack of some information in application note scatter file at link

    http://www.st.com/stonline/products/support/micro/files/an2078.zip

    . It should be corrected.

    lack line: * (+RW)

    Thank you for help.