Find attached an IAP project for RIDE. :-] it works fine :D Please note that you need some changes in your sections_FLASH.ld file in order to load some functions in RAM. You’ll find this modified file in RIDE folder. Copy it to C:\RIDE\LIB\STRX. Ensure that the original sections_FLASH.ld file is safe in other folder. Best regards, MBS [ This message was edited by: MBS on 28-03-2007 16:23 ]
does anyone have the IAP project for RIDE? I tried to use the IAP project supplied by ST (for IAR) and compile it with Kickstart version of IAR. The compiling was without errors, but after loading the hex into STR912 Flash Bank 1 by CAPS the processor doesn't do anything. The boot from bank 1 and bank remapping was set in CAPS according to supplied application note. I'm not sure of my Kickstart version of IAR, if there is everything configured as should. Due this reason I would appreciate functional project of IAP for RIDE.