I am new in IAP and have one question. I know that access and execution in sector0 is impossible during write or erase operations in sector 1 or 2. It means that my write/erase routines should be executed in RAM. May I execute another part of my bootloader in sector 0? For example, such way: 1) RS232 routine(reception of code) -- execution in sector 0 2) flash write routine -- execution in RAM 3) RS232 routine(reception of next code) -- execution in sector 0 4) flash write routine -- execution in RAM and so on My micro is ST7MC. Tnx in advance
I have an experience with ICC protocol and ST7F321. I transfer the program that is execute in RAM via ICC pin. With this solution you can reprogram all sector. In the ST7F321, there are lot of ram so I suppose that the RS232 routine can be execute but in the ST7MC I don't know. how many RAM in this uC? bye. excuse for my basic english. ;)