Skip to main content
Visitor II
April 17, 2007
Question

ICC Cable Length

  • April 17, 2007
  • 5 replies
  • 1172 views
Posted on April 17, 2007 at 07:41

ICC Cable Length

    This topic has been closed for replies.

    5 replies

    upamir2Author
    Visitor II
    April 6, 2007
    Posted on April 06, 2007 at 10:08

    Have a good day

    The icc cable between programmer and PCB, How long can it be.(maximum without mistake)

    İ use reva board v1 and st7fliteus5

    Visitor II
    April 16, 2007
    Posted on April 16, 2007 at 15:00

    Hello,

    one ICC cable is provided with Reva starter kit. Raisonance is sure that

    it works with it but doesn't give any guarantee for longer one because

    they didn't make serious test (stress) on that feature. For information,

    ST made some Lite09 programming tests with Stick and different ICC cable

    length four years ago. No problem has been found with 30cm, 1m, 2m and

    3m cables.

    It doesn't mean results are identical with RLink, it depends on PC and

    environment, i recommend you to make some tests.

    Best regards

    Pascal

    upamir2Author
    Visitor II
    April 17, 2007
    Posted on April 17, 2007 at 05:20

    Have a good day

    are the test cables longer than 1m shielded.

    i use not shielded 60cm and sometimes ''there is no mcu''.

    thanks for your interest

    Visitor II
    April 17, 2007
    Posted on April 17, 2007 at 07:37

    Hi,

    The ST-STICK is different comparing with the R-Link : STICK is plugged through parallel port with only passive components but R-Link is connected through USB and there is a ST7 onside the Rlink to interface between USB and ICC connection.

    Raisonance guarantee only with the ICC cable provided, but you have also to take care about the length on your PCB itself.

    Anyway, are you sure that no error will occur with a smaller ICC cable.

    Depending on your constraint you can rather increase the USB cable length.

    Best regards

    Laurent

    upamir2Author
    Visitor II
    April 17, 2007
    Posted on April 17, 2007 at 07:41

    nearly 40 cm is ok.

    Thanks for your interest