Skip to main content
Visitor II
May 4, 2004
Question

ICP on ST7SCR

  • May 4, 2004
  • 5 replies
  • 1075 views
Posted on May 04, 2004 at 14:05

ICP on ST7SCR

    This topic has been closed for replies.

    5 replies

    Visitor II
    April 26, 2004
    Posted on April 26, 2004 at 12:02

    Hi, FAE from Italy here.

    A customer is asking me if there is a low cost approach to the In System Programming of ST7SCR. I noticed that there is not a driver to program this micro neither in STVisualProgrammer nor in Softec Datablaze, selecting respectively ST7Stick and STX-INDART as HW tools. This is strange considering that ST7SCR is a HD flash device.

    More, I didn't find on STM pricelists ST7MDTS1-EPB2, is this tool available?

    Best Regards

    E.C.
    Visitor II
    April 27, 2004
    Posted on April 27, 2004 at 06:21

    For ST7SCR the EPB is available.

    The part no for EPB is - ST7MDTS1-EPB/EU, ST7MDTS1-EPB/UK, ST7MDTS1-EPB/US
    Visitor II
    April 29, 2004
    Posted on April 29, 2004 at 06:17

    Due to it's particular structure (without RESET pin) and ICC entry mode, the ST7SCR can't be programmed by SofTec Microsystems inDART-STX, but only with our gang programmer MP8011A, which controls the Vdd line to generate a power-on reset.

    Regards,

    Nicola
    Visitor II
    May 4, 2004
    Posted on May 04, 2004 at 13:56

    I think it could be possible using a indart ST7F ICD to perform this task. In particular the Reset signal coming from the ICD could be used to give the Vdd to the board (by a pushpull driver as an example). And selecting ST7F62x on DataBlaze interface (it seems this microes has the same bootloader start-up as ST7FSCR).

    Has anybody already done it?

    Regards

    E.C.
    Visitor II
    May 4, 2004
    Posted on May 04, 2004 at 14:05

    The scr uses a different bootloader, the icc pins are different for a start, aswell as the actual flash register is in a differant memory location.

    Flashbash currently supports the rom scr (with a reset pin).

    I am working on a solution for the flash variant (without reset pin).

    Regards

    sjo

    [ This message was edited by: sjo on 04-05-2004 17:37 ]