Skip to main content
Visitor II
October 21, 2003
Question

In-System JTAG Debugger for uPSD32xx

  • October 21, 2003
  • 2 replies
  • 537 views
Posted on October 21, 2003 at 20:13

In-System JTAG Debugger for uPSD32xx

    This topic has been closed for replies.

    2 replies

    igorlAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:56

    Hello!

    Another question concerning uPSD. I have the information from 3rd party developing company, that ST was to produce a JTAG debugger which costs only 100-200$. This part was proposed to use the same Flash-link interface as it uses now for ISP.

    Will you answer, when is this part is availible?

    Thank you very much in advance.
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:56

    Yes, ST and Keil developed a JTAG debugger called ULINK (under $200), however, it is for debugging the Turbo uPSD 33xx family processors. You can find more information on ULink at:

    http://www.keil.com/ulink

    .

    As far as for uPSD32xx family, you can obtain emulator from Nohau, which is more pricy but works very well, or you can use a lower cost emulator from Manley ~$200 but some of the fuctions are not yet supported, such as memory tracing and memory paging. You can get additional information on Manley ME3200 at:

    http://www.manley.com.cn/english