Skip to main content
Visitor II
March 3, 2003
Question

inDART-ST7/521 kit : can not get out from the Cosmic startup file, crtsx.s

  • March 3, 2003
  • 2 replies
  • 1263 views
Posted on March 03, 2003 at 06:43

inDART-ST7/521 kit : can not get out from the Cosmic startup file, crtsx.s

    This topic has been closed for replies.

    2 replies

    Visitor II
    February 12, 2003
    Posted on February 12, 2003 at 18:26

    I have an inDART-ST7/521 kit configured to target a ST72521R9T. At first, I used V1.05 then I recently switched to V1.0.9.

    For both versions, I noticed that my ST72521 program was sometime stuck in the crtsx.s startup file (I use Cosmic).

    Other times, I have some communication errors using STVD and Data Blaze.

    I am sure of my Cosmic code because I have tested it on a ST7 EMU3 emulator. My Indart kit is also brand new.

    Any idea to explain these 2 issues ?

    Jojo

    Visitor II
    March 3, 2003
    Posted on March 03, 2003 at 06:43

    When you say you're stucked in the startup file, does that mean stuck on a particular source code line or stucked because of a reset for instance? Check if you're configured in H/W WDG for instance (or place a breakpoint on the first line of the startup to see if the program performs reset).

    Do not hesitate also to ask support from Cosmic or Softec!