Skip to main content
Visitor II
July 28, 2023
Question

Infrared-Intensity Data from STHS34PF80

  • July 28, 2023
  • 1 reply
  • 905 views

I’m trying to get streaming data from the following combination:

- Device: STHS34PF80

- Adaptor: MKI231KA

- Motherboard: STEVAL-MKI109V3

 

I’ve connected a terminal emulator (PuTTY) to the USB port and can connect.

 

I can type the following commands:

*setdb231KA (yellow light comes on)

*zoff

*odr06, which presumably gives me a 8 Hz ODR (I’m not sure if this is the way to write to the register)

* start

 

Nothing happens.

 

I know I’m communicating because:

*dev returns STHS34PF80

*ver returns V3.42.4

*board returns ProfiMEMSTool

 

I’ve read through:

- DS13916 STHS34PF80 Datasheet

- UM2116 STEVAL-MKI109V3 Professional MEMSTool motherboard for MEMS adaptor boards

- DB4783 STEVAL-MK1231KA Data brief

- AN5867 Application Note

 

Still don’t know what to do.

 

Can anyone give me the series of commands to stream the infrared-intensity data to the terminal emulator? From there I can write an application to detect swiping.

    This topic has been closed for replies.

    1 reply

    ST Employee
    September 14, 2023

    Hello @SophieA ,

    There has been a case created to resolve this question and we will be reaching out to you directly.

    Regards,
    Roger