Skip to main content
Visitor II
May 22, 2003
Question

Interrupts trigger in uPSD

  • May 22, 2003
  • 2 replies
  • 575 views
Posted on May 22, 2003 at 16:30

Interrupts trigger in uPSD

    This topic has been closed for replies.

    2 replies

    jgilAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:54

    hi,

    I need some more information regarding the interrupts triggering in the uPSD3200 .

    I don't know if INT0 and INT1 are triggered by positive level/edge (refer to page 38 of the uPSD321x data sheet ) or they're triggered by negative level/triggered ( refer bit IT0 of the register TCON at the table37 of datasheet).

    Thanks in advance for any comments.

    Regards,

    Jokin

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 11:54

    Hi,

    According to Table 37, when IT0 bit is SET, INT0 is triggered at the falling-edge. When IT0 bit is CLEARED, INT0 is triggered at the low-level. IT1 control bit works the same way for INT1.