Did you measure the IDD(1.8V) and IDDQ(3.3V) in your board? It can be a hardware problem. Or try to erase the flash and try to load the program again. Please do these tests and let me know. Best regards, mirou.
I'm complitely blocked in here... i can´t do anything!!! Fri Aug 22 13:41:50 2008: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 5.0 Kickstart\ARM\config\flashloader\ST\FlashSTR91x.mac Fri Aug 22 13:41:50 2008: DLL version: V3.90b, compiled Aug 21 2008 14:51:23 Fri Aug 22 13:41:50 2008: Firmware: J-Link compiled Jul 30 2008 11:24:37 ARM Rev.5 Fri Aug 22 13:41:50 2008: JTAG speed is using adaptive clocking (RTCK signal) Fri Aug 22 13:41:50 2008: Initial reset was performed Fri Aug 22 13:41:50 2008: TotalIRLen = ?, IRPrint = 0x..00000000000000000000000000000000 Fri Aug 22 13:41:52 2008: Fatal error: Invalid core Id. (0) have you ever seen this?... can anyone help with this?? thank you :-[
The problem was BootLoader became all messed up and i just used a SEEGER tool to upload it again to his place, and all went well. By saying that BootLoader was a mess, it was what i assumed once the j-Link couldn't sync with ARM becouse it was no RTC clock to do it. Hope it help =)