Is there a way to change the Teseo-LIV3F COM baud rate and not have it stored in NVM?
We are currently using the Ublox M8 receiver and are in the process of qualifying the Teseo-LIV3 as a possible replacement. One issue I'm having is the need to up the baud rate after initially connecting and configuring the receiver. The Ublox M8 defaults to 9600 at power up, so it would be nice to always have the Teseo do the same. Is there a way to change the baud rate, of the Teseo, and have it volatile (returns to 9600 with hardware reset)?