Skip to main content
Visitor II
September 12, 2008
Question

is there a way to program a MCBSTR9 without uv3?

  • September 12, 2008
  • 3 replies
  • 843 views
Posted on September 12, 2008 at 06:50

is there a way to program a MCBSTR9 without uv3?

    This topic has been closed for replies.

    3 replies

    michaelAuthor
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:55

    hello,

    is there a way to program an MCBSTR9 without the kind support of uv3? is there an external tool that can do the job? something like FlashMagic but working with ULINK...?

    thanks in advance!

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:55

    Hallo,

    The are many tools supporting the STR9 device programming.

    You can for example use the standalone JTAG programmer/CAPS tool from STMicroelectronics to programm all STR9 device families. The USB/JTAG adaptor working with this tool is RLINK from Raisonance or Flink from ST. For more info about the tool :http://www.st.com/mcu/familiesdocs-101.html

    Also you can use RFlasher (SW from Raisonance) to program the STR9 flash memories.

    The tools listed above are not for development purpose but only for programming target.

    Best Regards,

    Ibtissem.

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 09:55

    Hi,

    You can also try the Olimex USB - OCD Jtag adapter,if you board has a JTAG connector (should be the case).

    The Olimex JTAG adapter cost 50$, Open OCD is open source, and both is usable to program the FLASH or debug a STR912. I m using this solution, and really happy about the result

    Regards.